Floating (Network) License
A floating (network) license is locked to a license server, which is a host computer that manages a pool of available software licenses. This type of network-based licensing involves a server-to-client interaction in which a client computer is required to check out a license from a server computer in order to access the software application (one license at a time and at one site). This enables geographically-distributed users to share licenses across a common network. Each license is either perpetual (license does not expire) or subscription (license expires after a limited amount of time).
To request a free trial license, go to the Information and Technical Support menu ("?" icon in upper right corner of the application) and select License Management. From the license management screen, click Get Trial or Buy License and then click Request a free trial license.
Software Support Subscription
Each software license includes free software updates and support for the specific instrument application for the duration of your support subscription. A perpetual license includes software updates and support for the first year, after which support can be renewed annually for a fee. A subscription license includes software updates and support through the term of the license. The time-bound aspects of the perpetual license (license does not expire) and the subscription license (license expires after limited time) start at the time you add the software license to your KSM profile.
To check the current details, click
(Information and Technical Support) at the top right of the Function Generator application and select My Support Subscription.
Activate Your License on Server Computer
Once you have purchased your software license, you will receive a Software Entitlement Certificate from Keysight via e-mail. You will then redeem the entitlement certificate from within the PathWave BenchVue application and you will receive an e-mail with a software license (*.lic) file attached.
For more details on network licensing, including troubleshooting information, see the Keysight Licensing Administrator's Guide.
- Go to the Information and Technical Support menu ("?" icon in upper right corner of Function Generator application) and select License Management. From the license management screen, click Get Trial or Buy License and then click Purchase a license to purchase a Software Entitlement Certificate for the Function Generator application. You can choose either paper or electronic delivery of your entitlement certificate.
Note: Alternatively, you can also go to www.keysight.com/find/BenchVue to purchase a Software Entitlement Certificate for the desired PathWave BenchVue applications.
- After you have received your entitlement certificate, note the Order Number and Certificate Number. You will need these numbers later in this procedure.

- Go to Keysight Software Manager (KSM) web site to redeem your license. You will need to provide the Order Number and Certificate Number from the entitlement certificate (see Step 2 above). In addition, you will need to provide the MAC Address (not the Host ID) for the server computer..
Note: If you are a first-time user of KSM, you will be required to complete a one-time registration on the web site. - Your software license has now been redeemed. You will receive an e-mail from Keysight with a software license file (*.lic) attached. Save the license file to your local computer and make sure to note the location.
- Set up a floating license server and install the license.
Launch the PathWave License Manager (PLM) software application – if not already installed on your computer, go to www.keysight.com/find/PLM to download the application.
Note: If you are a first-time user of KLM or PLM, you may be required to create a myKeysight account. Depending on the specific type of license being activated, PathWave will automatically determine which version of KLM or PLM to launch.
Note:For information on floating license server, refer to the documentation provided with the PLM application.
Your floating license is now activated and the license server process is running on the server computer.
Request a License on Client Computer
To use a floating license on a client computer, you must check out the license from the server computer (one license can be checked out at a time and at one site). If the floating license is not already running on the server computer, see Activate Your License on Server Computer above.
- Go to the Information and Technical Support menu ("?" icon in upper right corner of Function Generator application) and select License Management. From the license management screen, click Install Software License and then select Connect to license server from the drop-down list.

- To specify the network connection to the server computer, you will need the Host Name (not the Host ID) and port number (e.g., "27009@host1.example.com"). Please contact your System Administrator to determine your server's host name.

- Click Verify Connection and Save to complete the license request process.
Borrow a Floating License
Some floating licenses can also be borrowed for a specified number of days to be used offline. Once you have borrowed a license, you can disconnect the licensed computer from the license server and continue to use the license offline for the duration of the borrow period. Note that some older floating licenses do not support borrowing.
- You must be connected to the network, with access to a license server that has floating licenses for the product that you need to use.
- You will choose the license or licenses to be borrowed and specify a return date. You can typically borrow a license for up to 365 days, or until it expires, whichever comes first.
- Once you have borrowed the license(s) you need, you can disconnect your local computer from the network and use the licensed product offline. No one else can use that specific license count during the borrow period; the server will report the license as being in use and will deny checkout requests for that license count.
- You can terminate the borrow operation in one of two ways:
- At any time, you can reconnect your computer to the network and return the borrowed license.
- If you do not return the license before the return date, the license will automatically be returned even if your computer is not connected to the network. Once the license is returned, you can no longer use the licensed product and the license server considers the license count available to be checked out or borrowed by another client.
- At any time, you can reconnect your computer to the network and return the borrowed license.
To borrow or return a floating license, you can use the Pathwave License Manager (PLM) software application – if not already installed on your computer, go to www.keysight.com/find/plm to download the application.
To borrow/return a license, you must be connected to the network with access to the license server from which you borrowed the license.
- To borrow/return a license, you must be connected to the network with access to the license server from which you borrowed the license.
- From PLM, click Borrow Licenses.
-
Choose the license or licenses to be borrowed by selecting them from the list.
- Schedule a return date by selecting a date from the calendar icon. You can typically borrow a license for up to 365 days, or until it expires, whichever comes first. (The administrator of the license server can further restrict license borrowing using an options file on the server.)
- Click Borrow Now.
Once you have borrowed the license(s) you need, you can disconnect your local machine from the network, and use the licensed application offline. No one else can use that specific license count during the borrow period; the license server will report it as being in use and will deny checkout requests for that license count.